Search FAQs
What should parameter bFr be set to if you are using a 50hz 400vac motor?
Issue:
Setting up bFr parameter for a 50hz 400vac motor.
Product Line:
ALTIVAR ATV61
Environment:
All
Cause:
Installation / Setup
Resolution:
Drive settings for bFr, nPr, UnS , nCr and nSP settings, should match the motor nameplate.
in this case bFr will be set to 50hz and UnS will be set to 400vac
Setting up bFr parameter for a 50hz 400vac motor.
Product Line:
ALTIVAR ATV61
Environment:
All
Cause:
Installation / Setup
Resolution:
Drive settings for bFr, nPr, UnS , nCr and nSP settings, should match the motor nameplate.
in this case bFr will be set to 50hz and UnS will be set to 400vac
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: