{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Demonstration and Sample Code for the Link Object feature in Vijeo Designer

Issue:
Does Schneider Electric offer sample code or a demonstration video for the Link Object feature in Vijeo Designer?

Product Line:
Vijeo Designer

Cause:
Configuration and installation.

Resolution:
Yes, please see the provided attachment for a sample project created in Vijeo Designer v6.1 SP3.1.

The following video provides a demonstration of how to Link Objects in Vijeo Designer 6.2

Schneider Electric Saudi Arabia

Attachment(s)

LinkObject_DemoApp.zipLinkObject_DemoApp.zip [34.04 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: