{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert - An error message appears when opening the Logical Device Type Editor or attempting to select measurements in Reports
Attempting to launch the Logical Device Type Editor fails with an error saying that a UNIQUE constraint on table @MeasurementUnits is being violated. When attempting to select a measurement when configuring a report in the Reports web application, an error in the System Log appears simlar to the following:

Source = ReportView_MeasurementHierarchy
Target = /reporter/Default.aspx
Category = Reporting View
Description =
Violation of UNIQUE KEY constraint 'UQ__#B7D7C19__D64A4126724005BB'. Cannot insert duplicate key in object 'dbo.@MeasurementUnits'. The duplicate key value is (http://rddl.xmlinside.net/PowerMeasurementconfiguration/measurement/1/#Average%20Voltage%20Line-to-Line%20High)

The root cause of both problems is the same - duplicate metadata for measurement units in the ION_Network database. Is not known how the duplicates get created.
To work around this issue, it is necessary to modify a stored procedure called spDAL_GetMeasurementHierarchyNodes in the ION_Network database as follows:

Changed the existing stored procedure:

INSERT INTO
@MeasurementUnits
SELECT
(SubjectNamespace + Subject) -- combine the namespace and the subject to form the full name
, Object
FROM
vTS_Triples
WHERE
Predicate = 'unit'

to be (changes are underlined) - put the 'DISTINCT' key word after SELECT:

INSERT INTO
@MeasurementUnits
SELECT
DISTINCT (SubjectNamespace + Subject) -- combine the namespace and the subject to form the full name
, Object
FROM
vTS_Triples
WHERE
Predicate = 'unit'

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.