Search FAQs
ATV312 Solar TF ( tank full ) fault. Please guide how to bypass tank full as liquid probe is not used for level sensing?
Tank Full " TF" is not a fault, it is a status indication in drive, which is arrived form the liquid probe, if installed.
If the customer is not using using liquid probe(water level sensor), they should change the parameter "LPA" to "NO". As default this parameter setting in drive is AI2, hence it should be changed to "NO" to avoid Tank Full "TF" indication. Refer the screen shot below for the parameter details.
![parameter parameter](http://infomanager.schneider-electric.com/library/SCHNEIDER_ELECTRIC/SE_LOCAL/APS/APS_GLOBAL/ATV312%20Solar%20-%20LP%20assignment.png)
If the customer is not using using liquid probe(water level sensor), they should change the parameter "LPA" to "NO". As default this parameter setting in drive is AI2, hence it should be changed to "NO" to avoid Tank Full "TF" indication. Refer the screen shot below for the parameter details.
![parameter parameter](http://infomanager.schneider-electric.com/library/SCHNEIDER_ELECTRIC/SE_LOCAL/APS/APS_GLOBAL/ATV312%20Solar%20-%20LP%20assignment.png)
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: