{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many BCPMs can the EGX gateway have downstream?
Issue
What is the maximum number of BCPMs the EGX gateways can have installed downstream?

Product Line
Branch Circuit Power Meter

Environment
BCPM installation

Resolution
EGX Gateways support a maximum of 32 Modbus TCP/IP client connections. Since the BCPM use two modbus addresses it will be able to read up to 16 BCPM units.

Schneider Electric Saudi Arabia