{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What's the detail meaning of M241 AI catriage TMC4AI2 filter level?

The numerical filtering function configurable for every input channel is a low pass first order.
The mathematic formula used is:
Measn =  K * Measn-1 + (1- K) * Valn
With: K is the filter efficiency,
Measn is the filtered measure at time n,
Measn-1 is the filtered measure at time n-1,
Valn is the actual input value measured at time n.
The sample time (from time n-1 to time n) is about 10ms.
Filter efficiencyFilter LevelCorresponding  K value
No filtering00
Smooth filtering1
2
0,750
0,875
Average filtering3
4
0,937
0,969
High filtering5
6
0,984
0,992

Schneider Electric Saudi Arabia

Attachment(s)

M218 integrated AI and M241 AI cartridge Filter.pdfM218 integrated AI and M241 AI cartridge Filter.pdf [48.14 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: