{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the M580 weighing module?
Issue:
Part number for the M580 weighing module


Product Line:
M580


Resolution:
The part number for the M580 weighing module is PMESWT0100. Itis a versatile and flexible weighing module controller, which can be used wherever weighing scales are to be used in the Schneider Electric Modicon X80 automation system.

Schneider Electric Saudi Arabia