{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Telefast base is used with the BMEAHI0812 HART module?
Issue:
Telefast base that is used with the BMEAHI0812 HART module


Product Line:
Telefast


Resolution:
The following Telefast base can be used with the BMEAHI0812 HART module:
ABE7CPA02
ABE7CPA03
ABE7CPA31

using the BMXFTA1522/3022 cable

Schneider Electric Saudi Arabia