Search FAQs
Video: How can you program the ATV21 or ATV212 drive so that you can run the drive without the motor?
Issue:
Configuring ATV212 Drive to Run Without Motor Connected
Product Line:
Altivar ATV21 ATV212 S-Flex enclosed
Environment:
All
Cause:
Need to test the drive to see if there is a problem with it or a need to run the drive open circuit without the motor connected to it.
Resolution:
Programming
Find F- - - Enter
Scroll to Output Phase Loss F605= 0 (deactivate)
Set supply voltage correction F307 to 2 (supply voltage uncorrected).
Now you can disconnect your motor leads, and run the drive open circuit to test.
Be sure to return the parameters to their original value once testing has been completed.
Configuring ATV212 Drive to Run Without Motor Connected
Product Line:
Altivar ATV21 ATV212 S-Flex enclosed
Environment:
All
Cause:
Need to test the drive to see if there is a problem with it or a need to run the drive open circuit without the motor connected to it.
Resolution:
Programming
Find F- - - Enter
Scroll to Output Phase Loss F605= 0 (deactivate)
Set supply voltage correction F307 to 2 (supply voltage uncorrected).
Now you can disconnect your motor leads, and run the drive open circuit to test.
Be sure to return the parameters to their original value once testing has been completed.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: