{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we offer a ATV212 in an enclosure that is IP55 rated?
Issue:
ATV212 Type 12 NEMA or IP55

Product Line:
ATV212

Environment:
480v models

Cause:
None

Resolution:
The ATV212 drive can be purchased with a IP code of 55.  Please use the following link for a list of available drives:
https://www.se.com/products/us/en/50000-ac-drives-and-soft-starts/50010-ac-variable-torque/60162-featured-altivar-212-ac-drive/

Schneider Electric Saudi Arabia