{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Error 1500 "Another Installation is in Progress you must complete the installation before continuing this one" when trying to install Vijeo Designer?
Issue
Error 1500 "Another Installation is in Progress you must complete the installation before continuing this one" when trying to install Vijeo Designer?

Product Line
Vijeo Designer

Environment
Vijeo Designer Buildtime Installation in Windows

Resolution
This is an InstallShield error message.  Most commonly, it means that another instance of InstallShield is running.  Go to the Windows Task Manager and end all processes for Msiexec.exe or Msiexec.exe *32.  Then run the install for Vijeo Designer again.

Schneider Electric Saudi Arabia