{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can M241/M218/M238/M221 PTO only use one output, and another PTO output be used as normal output?

No, for M241/M218/M238/M221, one PTO channel must use two outputs! Any PTO output can not be used as normal output when PTO is configured!

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: