Search FAQs
How can a Vijeo Designer project be imported into SoMachine 4x?
To import a Vijeo Designer project into SoMachine 4.x follow these steps:
1. Open an existing SoMachine project or create a new project.
2. Under SoMachine Central click on the top-left wheel and select Import... / Import Vijeo Designer Project...
3. Navigate to your Vijeo-Designer project file (*.vdz) and select Open
SoMachine 4.x full versions: SoMachine 4.1, SoMachine 4.1 SP1, SoMachine 4.2, SoMachine 4.3
1. Open an existing SoMachine project or create a new project.
2. Under SoMachine Central click on the top-left wheel and select Import... / Import Vijeo Designer Project...
3. Navigate to your Vijeo-Designer project file (*.vdz) and select Open
SoMachine 4.x full versions: SoMachine 4.1, SoMachine 4.1 SP1, SoMachine 4.2, SoMachine 4.3
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: