Search FAQs
What is an SOF fault code on the ATV12 drives?
Issue:
SOF fault code on the ATV12.
Product Line:
Altivar ATV12
Environment:
Any
Cause:
• Instability
• Overspeed associated with the inertia of the application
Resolution:
• Check the motor
• Overspeed is 10% more than Maximum frequency tFr page 57 so adjust this parameter if necessary
• Add a braking resistor
• Check the size of the motor/drive/load
• Check parameters of the speed loop (gain and stability)
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: