{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the MTBF on the BMXNRP0200?

Issue:
What is the MTBF on the BMXNRP0200?

Product Line:
BMXNRP0200

Resolution:
ProductMtbf 30° ContinuousMtbf 30° IntermittentMtbf 60° ContinuousMtbf 60° IntermittentMtbf 85° ContinuousMtbf 85° IntermittentNb Cpt MissingNb Cpt Missing * QtyNb Cpt Total * QtyRatio Nb Cpt Missing / Nb Cpt Total
BMXNRP02002118895.4621579125.2281394785.7331135803.479890993.217779988.0047133813.40%

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: