Modbus TCP server | Modbus TCP slave device |
Only configure IP address | Need to configure parameters and I/O mapping |
For Modbus TCP client, all %MW address of server can be R/W. | For I/O scanner, only %IW area (2~40 words) can be R/W, %QW area (2~40 words) are read only, and actual %MW address of slave device cannot be visited. |
No need to configure “Unit ID” | Unit ID (1~247) should be same the unit ID setting in Modbus TCP I/O scanner. |
No visualized list for communicated address. | Have a clear and visualized interface to monitor all communicated variables. |
The connection to one client may be closed when more than 8 connections are needed. | The connection to the Master client is never forcefully closed, when IPMaster Address is configured. |
Please see attached ModbusTCP Slave Device explanation document.
Released for: Schneider Electric Saudi Arabia




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.