Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Can a full height 0U PDU be installed into the NetShelter SX Colocation cabinet?
Issue:
There's a need to mount a full height 0U PDU into the NetShelter SX Colocation cabinet.

Product Line:
NetShelter SX Colocation

Environment:
All versions and serial ranges.

Cause:
There's a need to use a PDU other than those recommended for use in the cabinet.

Resolution:
The NetShelter Colocation cabinet does not support the use of a 0U PDU. For a full list of the PDUs that are compatible with the Colocation cabinet please see the NetShelter Compatibility Chart in Knowledge Base document FA158651.
 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: