{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Maximum table in a recipeDB
Issue

While using the RecipeDB with the factorycast HMI, exceeding the maximum number of tables will cause the module to fail, this was tested with an automatic SQL request.

Product Line

Factory cast HMI (WMY, NMW)

Resolution

The maximum number of tables should be limited to 6 with 50 variables of 2 octets per table to insure a stable system.

Schneider Electric Saudi Arabia