{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an APF fault on the ATV61 drive?

Article available in these languages: Spanish

Issue:
APF fault on the ATV61 drive

Product Line:
Altivar ATV61

Environment:
All with an CIC or controller inside card

Cause:
The drive will ramp up and then trip on APF fault.

Resolution:
The APF fault is a fault or error on the controller inside option card.  Try swapping or replacing the controller inside card that has an identical program inside the card.

Schneider Electric Saudi Arabia

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]