{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I get the pinout for the RJ45 modbus port on the ATS22?
Issue:
Pin out for the RJ45 modbus port.

Product Line:
Altistart 22

Environment:
All serial numbers

Cause:
Modbus RJ45 pinout

Resolution:
RJ45 Pin 4 = D1
RJ45 Pin 5 = D0
RJ45 Pin 8 = Common
See the attached file, excerpt from the ATV22 user manual, for a complete listing.

Schneider Electric Saudi Arabia

Attachment(s)
ATS22_user_manual_EN_BBV51330_01.pdf [196.34 KB]