Issue:
Converting the Flex58 to the ATV61/71 using Adapter plate?
Product Line:
ATV61 and ATV71
Environment:
Frame size 2 to frame size 8
Cause:
Converting from the ATV58/FLEX58 to the ATV61/71
Resolution:
The Adapter plate that is used for mounting the ATV61/ATV71 in the same foot print as the ATV58 cannot be used to replace the FLEX58 with the ATV61/71 . The foot print of the FLEX58 is different from that of the ATV58, this difference is not compatible with the mounting plate.
Converting the Flex58 to the ATV61/71 using Adapter plate?
Product Line:
ATV61 and ATV71
Environment:
Frame size 2 to frame size 8
Cause:
Converting from the ATV58/FLEX58 to the ATV61/71
Resolution:
The Adapter plate that is used for mounting the ATV61/ATV71 in the same foot print as the ATV58 cannot be used to replace the FLEX58 with the ATV61/71 . The foot print of the FLEX58 is different from that of the ATV58, this difference is not compatible with the mounting plate.