Does the 174CEV30020 Modbus to Ethernet Bridge contains an embedded webpage?
No... The 174CEV30020 Modbus to Ethernet Bridge has a Configuration Menu Page that can be accessed through either an RS232 Serial Terminal Emulation Program or over IP using a Telnet session program
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Modicon Momentum
Modbus
Modicon Quantum
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.