{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you run a ATV61 and ATV71 on a high leg, corner grounded, or ungrounded delta system?
Issue:
ATV61 and ATV71 using high leg, corner grounded or ungrounded delta system.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Needs to know if there is anything that needs to be done on the drive when using a high resistance to ground system?

Resolution:
You can use the drive on an high resistance to ground system however you will need to deactivate the ground connection on the RFI filter board.  See the examples below for the low horsepower drive and the high horsepower drives.


See Attachment


Schneider Electric Saudi Arabia

Attachment(s)
IT Corner Grounded System.png [274.72 KB]