{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the function of the "Cold Start Only" option in the Unity processor configuration?

Issue:
Function of the "Cold Start Only" in Unity Processors


Product Line:
Unity Pro/EcoStruxure Control Expert


Resolution:
Cold Start Only

If checked, this option forces the cold start of the application, instead of the normal warm start upon power cycle of the PLC.
By default, the Cold Start Only option is unchecked.
The Cold Start Only option is only supported since PLC V2.7

NOTE: The Cold Start Only check box is present only if the current selected PLC can support it.

Schneider Electric Saudi Arabia