undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the screen resolutions that are supported under Generic PC Runtime in Vijeo Designer v6.2?
Issue:
What are the screen resolutions that are supported under Vijeo Designer Generic Windows PC Runtime?

Product Line:
Screen resolution, 4:3, 16:9, aspect ratio, 1080p, 1080i, 720p

Environment:
Generic Windows PC Runtime, Vijeo Designer

Resolution:
Below are the list of display resolutions available for the generic PC runtime:
800 x 600 (SVGA)
1024 x 768 (XGA)
1280 x 720 (HD720)
1280 x 1028 (WXGA)
1366 x 768 (FWXGA)
1440 x 900 (WSXGA)
1600 x 1200 (UXGA)
1680 x 1050 (WSXGA+)
1920 x 1080 (HD1080)
1920 x 1200 (WUXGA)
2560 x 1600 (WQXGA)

Keep in mind that the limitation of the resolution usually depends on the graphics chip on the industrial PC and monitor that are used.  

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top