{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many devices can the EGX 300 log?
Issue
How many power meters can EGX300 log?

Product Line
EGX300
EGX100

Environment:
Powerlogic Ethernet Gateways

Cause

1 - How many devices can an EGX300 log?
2 - How many devices can an EGX300 log if you add 1 or more EGX100s?

Resolution
1. The maximum number is 32 which is the maximum number of devices that EGX300 can connect to.

2. The maximum number is 64.

Consider both communication data and bandwidth when determining how many devices to connect to an EGX.

Schneider Electric Saudi Arabia