{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ION 7650/7550 or ION 8600/8650 support two separate IP address
Issue
User wants to know if ION 7650/7550 or 8600/8650 meter can support 2 separate IP addresses

Product
ION 7650, ION 7550, ION 8600, ION 8650

Environment
Two separate networks wanting to connect to the same device

Cause
User wants to know if ION 7650/7550 or 8600/8650 meter can support 2 separate IP addresses

Resolution
The meters do not support multiple IP addresses.
1. The ION 7550/7650 meter can have Infrared and copper Ethernet ports but share the same IP address. Dual comm Cards are not supported.
2. The ION 8600/8650 meter will have either Infrared or copper Ethernet connections but not both.

Schneider Electric Saudi Arabia