{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I upgrade a project from Vijeo Designer V4.1 to V6.2?

Article available in these languages: Spanish

Issue
How do I upgrade a project from Vijeo Designer V4.1 to V6.2?

Product Line
Vijeo Designer

Environment
HMI Configuration software for Windows

Resolution

Step 1:
If the starting version of the project was from a version of Vijeo Designer equal to or greater than v1.0 and less than v4.3,
import the .VDZ project export file into v4.3

Step 2:
If the starting version of the project was from a version of Vijeo Designer equal to or greater than v4.3 and less than v4.6,
import the .VDZ project export file into v4.6 or v4.7

Step 3:
If the starting version of the project was from a version of Vijeo Designer equal to or greater than v4.6 and less than v6.1,
import the .VDZ project export file into v6.1

Step 4:
A project file that is version v6.1 (all patches and service packs) can be opened in any version of Vijeo Designer v6.2

Schneider Electric Saudi Arabia