{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can I return an inoperative drive or soft start under warranty?

Issue:
Return an inoperative drive or soft start under warranty.

Product line:
Altivar, Altistart

Environment:
All models

Cause:
Altivar drive or Altistart soft start does not work, and I want to return under warranty.

Resolution:
To return a drive or soft start product, the first point of contact needs to be the Drives Product Support group (DPSG).  The DPSG needs to create a case to document the part number, serial number and troubleshooting in order to set up a return.  The Drives Engineer can make the determination if the product is covered under warranty, and confirm appropriate troubleshooting steps have been taken.

The drive can be returned only or exchanged for the same product.  To return only, contact the Claims team with the case number.
For an exchange, contact the Drives Resale group in Raleigh with the case number and drive/soft start part number.
If you are an end user, you will need to contact a local distributor or point of purchase with the case number.

Attached is a copy of the Schneider Electric Drives and Soft starts Service Guide which covers this in more detail.

Schneider Electric Saudi Arabia

Attachment(s)

8800DB0101.pdf8800DB0101.pdf [599.35 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: