{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an absolute encoder be used on an Advantys Island?
Issue:
Can an absolute encoder be used on an Advantys Island?

Product Line:
Advantys

Cause:
To see if an absolute encoder can be used on an Advantys  island.

Resolution:
Yes, you can use any of the Advantys NIMS and use a CANopen extension  card STBXBE2100 and add the XCC-351xxS84CB Osicoder multi-turn absolute encoder.

Schneider Electric Saudi Arabia