Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Can the NetShelter SV be joined to a NetShelter SX?
Issue:
Customers are using the NetShelter SX and SV in a row based design.

Product Line:
NetShelter SV, NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers want to know if the SX and SV cabinets can be joined via baying brackets.

Resolution:
The SV frame does include joining holes and hardware for baying to other SV cabinets but alignment to non-SV cabinets may be difficult due to the different frame design of the NetShelter SV. The SV and SX cabinet depths are different. The front doors are also different shapes: the SV is flat and the SX is rounded. No height adapters are available for matching the height of the SV to ISX components. The SV cabinets are not designed to be used with ISX or EcoAisle.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: