{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
In the NetShelter CX Enclosure Brochure the number of outlets per cabinet does not match the number of ports on the PDU, why?
Issue:
The NetShelter CX Enclosure Brochure shows the number of outlets and it does not match the number of ports on the PDUs.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
The numbers actually decrease from the 18U, to the 24U, to the 38U cabinets.

Resolution:
The number of ports shown on this document is the number of AVAILABLE ports in each cabinet.
Each cabinet contains a different number of fan units which plug into the PDU. So, as the cabinets increase in size the number of available ports are reduced.
The 18U cabinet has one fan module, the 24U has two fan modules, the 38U has three fan modules.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.