{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why has my PME system CPU usage increased to almost 100%
Issue
Windows Task Manager performance view will  show high CPU usage 90% to 100% being constant over period of time. A further investigation of the running processes will show the WebReach.XMLSubscriptionService.exe*32 using 30% to 50% of CPU usage with high number of Handles and Threads.

Product Line
Power Monitoring Expert (PME) 7.x
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.0

Environment
Windows Task Manager

Cause
Windows Task Manager performance view will  show high CPU usage 90% to 100% being constant over period of time. A further investigation of the running processes will show the WebReach.XMLSubscriptionService.exe*32 using 30% to 50% of CPU usage with high number of Handles and Threads.

Resolution
Stopping WebReach.XMLSubscription service on PME server drops the high CPU usage. Web Applications Diagram (WebReach) user on the network is possibly using XML scraping process to pull real time data into third party system. Scraping XML process impacts performance of PME server and therefore not supported.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.