Issue:
There are measurements available on a device such as a device's serial number and volts mode. However these measurements are not available for selection in the real time tables
Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Environment:
Web Applications Real Time Tables
Cause:
Real Time Tables support only certain data types. The measurements that do not appear in the list of available measurements are of a type that is not supported.
Resolution:
Real Time Tables only supports the following data types: numeric, date, boolean.
String type such as device type, serial number and volts mode cannot be displayed.
There are measurements available on a device such as a device's serial number and volts mode. However these measurements are not available for selection in the real time tables
Product Line:
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Environment:
Web Applications Real Time Tables
Cause:
Real Time Tables support only certain data types. The measurements that do not appear in the list of available measurements are of a type that is not supported.
Resolution:
Real Time Tables only supports the following data types: numeric, date, boolean.
String type such as device type, serial number and volts mode cannot be displayed.
Released for:Schneider Electric Saudi Arabia