{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: How to place Symmetra PX back online from Maintenance Bypass (MBP)

Article available in these languages: Spanish

Issue:
How to place Symmetra PX back online from Maintenance Bypass (MBP)

Product line:
Symmetra PX 20K,40K, 80K, 100K

Environment:
All Product models, all serial numbers

Cause:
This video provides a step by step instruction on how to operate the Symmetra PX UPS from Maintenance Bypass mode, to allow the end-user to transfer load back to the UPS without interruption.

Resolution:
Preconditions: PDU with Maintenance Bypass breakers Q2 is open, Q3 is closed, UPS is in Static Bypass operation, bypass LED on display is illuminated, H2 light over Q2 should be on, H3 light over Q3 should be off.
  1. Close Q2, H2 light over Q2 and H3 light over Q3 should be on
  2. Open Q3 switch, H3 light over Q3 should remain on and H2 light over Q2 should now be off
  3. Go to the UPS display under the "Control" menu; take the UPS out of Bypass
The green "Load On" light on the UPS display should be illuminated and H2, H3 Lights should now be off over the Q2, Q3 switches in the PDU with Maintenance Bypass.

Video 1

Schneider Electric Saudi Arabia

Attachment(s)

UPS BYPASS SEQUENCE.pdfUPS BYPASS SEQUENCE.pdf [90.24 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: