Search FAQs
Can an AR3100 be converted into an AR3200 Colocation cabinet, or can the Colocation doors be installed onto an AR3100?
Issue:
Customer requests the upper/lower door design of the NetShelter Colocation cabinet on a NetShelter SX cabinet.
Product Line:
NetShelter SX AR3100, AR3300
Environment:
All versions and serial ranges.
Cause:
For various reasons the customer may want the NetShelter Colocation under/over style door mounted onto a NetShelter SX cabinet.
Resolution:
Currently the Colocation door design is compatible with the NetShelter Colocation cabinets only. It is not compatible with the NetShelter SX cabinets. There are no special adapters to allow the NetShelter Colocation doors to mount onto the NetShelter SX frame.
Customer requests the upper/lower door design of the NetShelter Colocation cabinet on a NetShelter SX cabinet.
Product Line:
NetShelter SX AR3100, AR3300
Environment:
All versions and serial ranges.
Cause:
For various reasons the customer may want the NetShelter Colocation under/over style door mounted onto a NetShelter SX cabinet.
Resolution:
Currently the Colocation door design is compatible with the NetShelter Colocation cabinets only. It is not compatible with the NetShelter SX cabinets. There are no special adapters to allow the NetShelter Colocation doors to mount onto the NetShelter SX frame.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: