{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the sharing field (none, read only, or read/write) of the variable property in Vijeo Designer pertains to the Magelis access the PLC tags?
Issue:
Is the sharing field (none, read only, or read/write) of the variable property in Vijeo Designer pertains to the Magelis access the PLC tags?

Product Line:
Vijeo Designer

Resolution:
No, the sharing field in Vijeo Designer is for data sharing which is used for Web Gate.

Schneider Electric Saudi Arabia