{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I Start and Stop the motor using the speed reference?

Issue:
Is it standard practice to use the speed reference to start and stop the drive while keeping the run command activated?

Product Line:
Altivar drives

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
No, it is not recommended to start and stop using the speed reference. When the run command is activated, the output transistors are biased ON. This can increase the opportunity for voltage transients to cause damage. It is recommended to use a switch or relay to deactivate the run command (Digital Input) when the drive is not called to run the motor.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: