{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to transfer program from one ATV212 to another with different horsepower ratings using SoMove?
Issue:
Transfer program from ATV212 to an ATV212 with different horsepower ratings using SoMove?

Product Line:
Altivar 212, Altivar Machine

Environment:
All

Cause:
Copy programming between drives of different sizes.

Resolution:
No, it is not possible to transfer files between drives with different horsepower ratings.  The reference (part number of the drive) must match.

Schneider Electric Saudi Arabia