ATV-IMC" is always 00:00 01/01/2000 | Schneider Electric Saudi Arabia" />
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Time in ATV71 keypad under "DriveMenu -> ATV-IMC" is always 00:00 01/01/2000
This is because time is not synchronised between ATV71 and IMC card.

To enable time synchronisation the following program line should be added to ATV_IMC_Start POU:
DriveFaultDatation(Activate:=TRUE );

Schneider Electric Saudi Arabia