{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where are the Non-Resettable faults listed in the ATS22 manual?
Issue:
List of Non-Resettable faults on ATS22.

Product Line:
ATS22

Environment:
All

Cause:
Need to know all faults that are resettable

Resolution:
This information is provided in the ATS22 User manual. The information is in the part of the LI2/LI3 configuration section on page 60 of the Sep 2015 manual.

PIF (Phase Inversion fault), PHF(Input phase loss), SCF(short circuit), CFF(ATS invalid configuration) and trAP(error code) cannot be reset in case of a fault. If the fault condition disappears and the ATS22 is powered ON, normally there is no problem restarting the ATS22.

Schneider Electric Saudi Arabia