{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.

Issue
Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.

Product Line
ProWORX 32

Environment
Windows 7,Windows 8, Windows 10

Resolution
McAfee Anti-viirus software detects 'Credit.exe' as an infected file.

The 'Credits.exe' file is only used to present a 'Thank for using ProWORX 32' pop-up message window.  The file is
not used in any part of the ProWORX 32 software.  It can be deleted.  The file should be deleted using the delete
function in the anti-virus software.

Attempts to delete the file from a folder may fail.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: