{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause an EPF fault on the Altivar ATV31 and ATV312 drives?
Issue:
EPF fault on the Altivar ATV31 and ATV312 drives.

Product Line:
Altivar ATV31 and ATV312

Environment:
All

Cause:
Drive is tripping on EPF fault on power up?

Resolution:
EPF is an external fault.  Check your logic inputs in the FLT menu  code EtF to see if its an logic input.

Schneider Electric Saudi Arabia