{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the dimensions of the Line Choke for a size 10 ATV61/71 drive?
Issue:
Dimensions of the Line Choke for a size 10 ATV61/71 drive.

Product Line:
ATV71HC11N4, ATV71HD75M3X, ATV61HD90M3X, ATV61HC13N4

Environment:
Size 10 ATV61/71 HHP drives

Cause:
DC chokes for Size 10 ATV61/71 drives

Resolution:
The part number is VW3A4559.
Dimensions:
Width- 320 mm
Height=380 mm
Depth-210 mm
Note: This choke is NOT installed in an enclosure ( For open style units).

Schneider Electric Saudi Arabia