{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the input voltage tolerance on the ATV61 and ATV71 series drives?
Issue:
Input voltage tolerance on the ATV61 and ATV71

Product Line:
Altivar 61 & 71

Environment:
All models, All serial numbers.

Cause:
Input voltage tolerance range needed.

Resolution:
For single phase input, part # ATV61H075M3 through ATV61HU75M3:  200 -15% to 240 +10%
For three phase input, part # ATV61H***M3 and ATV61H***M3X:  200 -15% to 240 +10%
For three phase input, part # ATV61****N4 and ATV61W***N4C:  380 -15% to 480 +10%
For three phase input, part # ATV61H***Y:  500 -15% to 690 +10%


For single phase input, part # ATV71H075M3 through ATV71HU75M3:  200 -15% to 240 +10%
For three phase input, part # ATV71H***M3 and ATV71H***M3X:  200 -15% to 240 +10%
For three phase input, part # ATV71****N4 and ATV71W***N4C:  380 -15% to 480 +10%
For three phase input, part # ATV71H***Y:  500 -15% to 690 +10%

Schneider Electric Saudi Arabia