{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV212 or S-flex drive is running full speed with PID enabled drive does not appear to be responding to the PID feedback.
Issue:
ATV212 or S-flex drive is PID does not appear to be responding to the PID feedback.

Product Line:
Altivar ATV212 S-flex

Environment:
All

Cause:
Drive is running full speed and is not responding to the PID feedback

Resolution:
Troubleshooting Tips:  Check the PID feedback signal 1st to see if the drive is getting good feedback.
Check the programming F360 make sure its set to the PID feedbacks input.  VIA-1 or VIB-= 2

Schneider Electric Saudi Arabia