{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
BMXFTW301 cable diameter
Issue
This Resolution provides the maximum diameter for the BMXFTW301 cable.



Product Line
BMXFTW301



Resolution
The maximum BMXFTW301 cable diameter is 9.5mm


The BMXFTW301 is a cable used with M340 I/O modules.  It has a 20 pin terminal block on one end and color-coded flying leads on the other end.




Schneider Electric Saudi Arabia