{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the new 6U, 9U and 12U NetShelter cabinets hinged in the rear, like AR100 & AR100HD?
Issue:
Customers inquire if the newer 6U, 9U and 12U wall mount cabinets are hinged in the rear.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The 13U NetShelter WX cabinets are hinged in the rear.

Resolution:
The new 6U, 9U and 12U NetShelter WX cabinets (AR106, AR109, AR112) are not hinged in the rear. Only the NetShelter WX AR100 and AR100HD are hinged in the rear,

Schneider Electric Saudi Arabia