{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you program the ATS22 softstarter to trip if it exceeds some number of starts per hour?
Issue:
How can ATS22 be programmed for a fixed number of starts per hour?

Product Line:
Altistart ATS22

Environment:
All

Cause:
Wants to delay the total number of times the softstarter can be started in one hour.


Resolution:
Programming:
Adj menu
Snb= number of starts  Off or 1 thru 10
SLG= Start period 1 min thru 60 mins

Example= if Snb= 3 and SLG is 10 mins   you can start and stop the drive 3 times in 10 mins.  If you exceed the programmed start time the drive will trip out on SnbF.

Schneider Electric Saudi Arabia

Attachment(s)
ats22_user_manual_en_bbv51330_02.pdf [3.02 MB]