{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Simple example of MBP_MSTR write using function 1 (with abort/reset) Ethernet communication for Quantum
Issue

I need a simple example of MBP_MSTR write (with abort/reset) Ethernet communication for Quantum
Product Line
Quantum, Control Expert, UnityPro

Environment
Windows 7, Windows 10

Resolution

The Ethernet communications can be confusing to program using Unity, since they vary from PAC family to family. This is one of a series of example applications that presents each function block in a working version for the user to build on.
The attached application mbpmstrf1.zef will write ten registers to another device (using MBP_MSTR function 1). The application consists of three sections. The first is an ST section in which variables are initialized. The second section, which is the example proper, is a LD section which uses an MBP_MSTR function block to write 10 registers to another device, the server. The IP of the server is 192.168.1.30. This should be changed to suit your own addressing scheme. There is also code in that section to time the response. The MBP_MSTR block does not contain a timeout. It is good practice to program your own application timeout. The timer can be set to an appropriate value. If the timer expires the application issues a reset of the connections to the server. This can be seen in section 3.  The application is annotated and should provide a start for the user of the MBP_MSTR block. It is up to the user to change the PAC type and IP addresses to meet his or her own requirements. There is both a .zef and .xef version in the zip file.

Schneider Electric Saudi Arabia

Attachment(s)
function1.zip [61.89 KB]